Skip to main content
Visitor II
July 24, 2023
Question

SPSB081-Component Datasheet

I am working on SPSB081 power management control IC. I need support in the following points:

1. which revision of data sheet to be followed, because there are some discrepancies in register set(addresses) of revision 2 datasheet.

2. for refreshing the watchdog, TRIG bit should be toggled every time within safe window(7.5 to 12 ms in configuration1, 37.5 to 60ms in configuration2), though i am toggling the TRIG bit of CR1 register for every 50ms, still the NRESET pin is toggling which means reset is happening. 

can some one help me in the above points???

This topic has been closed for replies.