Skip to main content
Cooke.Ernest
Associate III
April 18, 2017
Question

SPINFamily Evaluation Software - BEMF Calculation

  • April 18, 2017
  • 8 replies
  • 1971 views
Posted on April 18, 2017 at 14:07

Hi,

When I am using the BEMF compensation configuration within the SPINFamily Evaluation Software, I input the Application Parameters and the Motor Parameters for my particular motor. 

0690X00000606nmQAA.png

When I press the �Evaluate� button at the bottom right of the menu, the following Device Configuration Values are calculated:

KVAL_HOLD

KVAL_ACC

KVAL_DEC

KVAL_RUN

ST_SLP

INT_SPEED

FN_SLP_ACC

FN_SLP_DEC

These calculated values can then be written to the device and can be seen in the Phase current control tab within the �Device Configuration� menu.

 0690X00000606nnQAA.png

How are the Device Configuration Values calculated from the values that I have inputted?

Is there a particular calculation that must be used?

Kind Regards,

Ernest

#dspin #dspin-gui #powerstep01 #bemf #pcc009v2-eval6470h-spinfamily
This topic has been closed for replies.

8 replies

Enrico Poli
ST Employee
April 19, 2017
Posted on April 19, 2017 at 15:09

Hi,

the calculations performed by the tool are the ones described in details into the

http://www.st.com/resource/en/application_note/dm00061093.pdf

.
Cooke.Ernest
Associate III
April 20, 2017
Posted on April 20, 2017 at 14:39

Hi Enrico,

Thank you very much for the information you have sent me in relation to the calculations.  I found them to be helpful.

There are some further questions I would like to ask. 

From the values I have entered I was able to calculate the Hold duty-cycle, Intersect Speed & Starting Slope perfectly.

I got a value of 30% for the acceleration, deceleration and run duty cycles instead of 46.5% (See below).

However I was unable to calculate the Final Slope Values (Acceleration & Deceleration).  

Is it possible you could find the values which I am unable to calculate properly.  The parameter values to input are shown below.

0690X00000606aBQAQ.png0690X00000606pOQAQ.png

Thanks,

Ernest

Enrico Poli
ST Employee
April 26, 2017
Posted on April 26, 2017 at 14:43

Did you considered the conversion between rms current and peak?

Can you write your calculation?

David Walker
Associate
April 19, 2017
Posted on April 19, 2017 at 18:55

I came up with an alternative way to compute the motor parameters. It is here:

https://community.st.com/0D50X00009XkW2fSAF