Skip to main content
tobias239955_st
Visitor II
October 21, 2014
Question

SPI communication problem

  • October 21, 2014
  • 1 reply
  • 558 views
Posted on October 21, 2014 at 15:30

hello,

I have a EVAL6480H board and try to connect it with a Atmel Xmega. But on the SDO line is always the Byte which I send before on SDI.

Does I Need to make some initalisation before start a communication?

I choose SPI Mode 3 and a frequency of 250kHz.

Hope someone can give me advise. 

#l6480 #l6482-spi #spi-config-problem
This topic has been closed for replies.

1 reply

xbd_119
Visitor II
January 24, 2016
Posted on January 24, 2016 at 05:01

Hi,

 Is it solved?

 I have meet the same issue with the board 

EVAL6482H, my MCU is the dsPIC30F5011,  i 

also checked all the SPI signals, they are all flowing the spec.

 anyone can help ?