Question
Speed Control according to DT0001
Posted on March 11, 2015 at 10:54
Hi,
the application note DT0001 suggests controlling the motor speed by using the FWD/REV pin with a duty cycle. Though this sounds very promising especially for feed-back controller design I was wondering what happens if the motor is running in one direction and I force the motor to drive the other way. Isn't the motor than used in generator mode acting as a voltage source? Has anyone had experience with this usage and how is the L6235 reacting to it - where is the power burned? Thanks, Rasmus #brushless-speed-control #l6235 #dt0001