Welcome, @NHiel.1, to the community!
The value is a pulse value, which is also only guaranteed at the said pulse values.
To be more precise, the 600W also only applies for a limited time, namely the 10/1000μs pulse mentioned in the data sheet, where 10µs refers to rise time tr and 1000µs to the pulse duration td. For the 4kW mentioned, this is tr=8μs and td=20µs.
The shorter the pulse, the higher the power the TVS can handle without thermal damage to the chip, as this may only happen with a very low duty cycle.
You will find more details in e.g. AN316.
Does it answer your question?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.