Skip to main content
MSmit.8
Visitor II
Aug 26, 2021 4:38 PM UTC
Solved

SMAJ Peak Pulse Power over Pulse Duration Curve

How is the curve in Figure 4 in the datasheet measured? I noticed in Figure 5 that the 20 us pulse has a 8 us rise time and the 1000 us pulse has a 10 us rise time. The 10 ms pulse doesn't even have a specified rise time. Is each point in the Figure 4 graph just a standardized square wave with the same rise time and incrementing the pulse width, or does each measurement have a different rise time? If so what is the rise time for the pulses measured?

    This topic has been closed for replies.
    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Aug 31, 2021 12:53 PM UTC

    Welcome, @MSmit.8​, to the community!

    as you can also find in AN316 only pulses of 8/20µs (IEC 61000-4-5) and 10/1000µs (IEC61643-123) are stardardized and mentioned in table 3 of the datasheet, the curve with 10ms just gives an idea of the maximum current.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

    1 reply

    Peter BENSCH
    Peter BENSCHBest answer
    ST Technical Moderator
    Aug 31, 2021 12:53 PM UTC

    Welcome, @MSmit.8​, to the community!

    as you can also find in AN316 only pulses of 8/20µs (IEC 61000-4-5) and 10/1000µs (IEC61643-123) are stardardized and mentioned in table 3 of the datasheet, the curve with 10ms just gives an idea of the maximum current.

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.