Skip to main content
Whanni
Visitor II
April 23, 2019
Question

Shorted between VDD and VSS, what are causes? How can it produce?

  • April 23, 2019
  • 1 reply
  • 1858 views

Currently, I design a board with STM32f413 to Motor control. Sometimes, when I turn on the power supply , I have a shorted occurs betwwen VDD (+3.3V) and VSS. So I had to change my CPU to my board. In my board, I have a different power supply betwen my VDD and VDDA.

0690X000008AoaWQAS.png

Do you think a separated power supply can produce a shorted if the VDD and VDDA are not provide at teh same time? Or if there are drop between it?

Thank you,

Best regards,

Wh

This topic has been closed for replies.

1 reply

Uwe Bonnes
Chief
April 23, 2019

I managed to get "hot" STM32 by injecting to much current into some input. I read the datasheet 6.1.7. that as long as every voltage is below 4.0 volt, either VDD or VDDA can be omitted with no harm. Check your layout for: Spikes in VDD(A) when switching, unconnected VDD(A) pins, or pins unintentional connected to voltage > 4 Volt.