shape of current waveforms measured at shunt
So, I'm expecting the voltage developed across the shunt resistor to be sinusoidal, but I'm having much difficulty measuring these on the STEVAL-ESC001. The shunts on that board are 10mOhms, and perhaps the current through the motors is too low to see anything useful with the scope.
Am I correct in expecting this waveform to be sinusoidal, if the BLDC is a SPMSM? I am running the motor unloaded, and perhaps that is why it is not drawing much current at 10K rpm. I can increase the value of the shunt resistor to see if I can see this waveform.
Does anyone have a current profile for whatever motor they're using they can share so I can see what to expect? from start to constant speed to stop (or ramp down). The motor I'm using at constant speed is drawing less than 250mA, at 8000 RPM.
Thank you
Jorge