Skip to main content
JD.1720
Associate
Feb 28, 2021 7:42 PM UTC
Solved

sensored BLDC motor for X-NUCLEO-IHM16M1

I recently purchased the NUCLEO-F303RE and X-NUCLEO-IHM16M1 development kit.

With a 2804 Gimbal motor.

So far all the tests have gone well for me.

But my intention is to control a sensored BLDC motor.

Do you know of any sensored BLDC motor that works well with this development kit?

Thanks!

This topic has been closed for replies.
JD.1720
JD.1720Best answer
Associate
Mar 24, 2021 7:50 PM UTC

I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.

3 replies

Cristiana SCARAMEL
ST Employee
Mar 2, 2021 8:30 AM UTC

Hello @JD.1720​ and welcome to the ST Community.

I cannot suggest a brand but only to choose a three-phase brushless motor with compatible voltage and current for the STSPIN830 driver.

If you want to use the kit power supply the voltage ratings is reduced to 12 V (nominal value).

Otherwise you can use an external power supply with output voltage between 7 and 45 V (CN1 or Ja connectors).

Concerning the X-NUCLEO-IHM16M1 hardware settings you can refer to the user manual UM2415.

Let’s see if other Community Members can suggest you a specific motor part number that they used.

"If you feel a post has answered your question, please click ""Accept as Solution"""
JD.1720
JD.1720Author
Associate
Mar 17, 2021 7:55 PM UTC

Thanks for help

JD.1720
JD.1720AuthorBest answer
Associate
Mar 24, 2021 7:50 PM UTC

I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.