Skip to main content
joe_electric
Visitor II
May 8, 2023
Question

Sending serial data via SBU when STUSB4500 has negotiated PDO3

I'd like to use STUSB4500 to allow for 20V 60+W to enter the system, but I'd also like to use the sideband pins (or other pins) to send some serial data to the host side. I'd like to know whether this is possible (seems like the chip doesn't use SBU pins to deliver power), and whether this use of SBU during PD is compliant with USB specs.

    This topic has been closed for replies.

    1 reply

    NBALL
    ST Employee
    May 15, 2023

    hello

    STUSB4500 manages only power negotiation with source and does not handle USB3/USB2 or SBU pins.

    BTW SBU is generally used in some Alternate modes which are not supported by stusb4500

    Best regards

    Nathalie