Skip to main content
Visitor II
November 23, 2024
Question

SCT1000N170AG_V2 SPICE model uses help

Dear Engineer:

Is there an error in the SPI model of SCT1000N170AG_V2?

Why do I have such a simple switching circuit, and when SCT1000N170AG_V2 is turned on, the waveform is like this? Theoretically, the conduction should be 500V, and the output should be a square wave with a period of 20us, a duty cycle of 50%, and an amplitude of 500V.

JAYCE_0-1732366799730.png

We look forward to your reply, thank you very much.

*This post has been translated from Chinese to comply with the ST Community guidelines.

This topic has been closed for replies.