Skip to main content
Visitor
September 23, 2026
Question

RHFL4913 OCM sink current

  • September 23, 2026
  • 0 replies
  • 11 views

Hi

I’m looking for the maximum sink current capability on the OCM pin of the RHFL4913, and I find some inconsistency between two information available in the last datasheet (rev 22 dated of july 2025).

  • At the end of the table 5 (§4) I get a 0.38V voltage value for a 24mA sinked current in the pin.
  • But in the §7.5 I find a 10mA sink current value.

Which one can I consider as the maximum sink current value ?

Thanks for your help.

Regard