Skip to main content
Visitor
September 23, 2026
Question

RHFL4913 current limitation value

  • September 23, 2026
  • 0 replies
  • 11 views

Hi

I have a question about the current limitation embedded in the RHFL4913, as there is an inconsistency between two information in the last datasheet (Rev22).

  • in the Table 5 (§4), we can find the “Iolim” (overcurrent protection limitation) range defined as 0.8A minimum and 2A maximum.
  • In the §5 (Figures 42 and 43) we can see that the minimum recommended value for “Ish” is about 0.75A. If we divide this value by 1.6 to get the corresponding “Iolim” value, we obtain 0.47A. This is not consistent with the 0.8A value found in the table 5.

Can anybody help me with this problem ? Maybe the Figures 42 and 43 are considering “Iolim” instead of “Ishadj” ? Or there is a mistake in the Table 5 ?

Thanks for your help

regards

Philippe PELEGRI