Skip to main content
Associate
February 7, 2025
Question

Reverse Polarity with ST1S14

EN11_0-1738929544771.png

Hello I have created reverse polarity but it can not work stable especially in the first work , this time I change the voltage a little bit it works :) ı cant understand.

What should ı do?

This topic has been closed for replies.

2 replies

Peter BENSCH
ST Technical Moderator
February 7, 2025

Welcome @EN11, to the community!

  • What output current do you want to draw at -15V_O?
  • What is the saturation current of L2?
  • Can you please show the layout so that this can be checked?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
EN11Author
Associate
February 7, 2025

I am using the just supply for opamps , and also ı guess understand problem is a lot capacitors ı put the resistor in the output problem seems to be solved.

but ı continue to try .

Best Regards.