Skip to main content
Associate
October 17, 2024
Question

Question on Gate driver VNQ860SPTR-E

I want to know about the compatibility check between the gate driver ic VNQ860SPTR-E and microcontroller PIC32MZ1024EFH144-I/PL 

Can I use this gate driver for my above mentioned microcontroller.

This topic has been closed for replies.

9 replies

Richard Li
Senior
October 17, 2024

So powerful Microchip should no problem.

For detail check-compatibility, do you want use two GPIO for one gate driver pin like datasheet noticed?

If this no problem, one input GPIO detect overtemperature interrupt.

If you one use one GPIO for one gate driver pin, change between in and out, you can't set interrupt, this may cause problem for overtemperature response time.

The Microchip voltage is 2.1-3.6V, if you can keep >3.3V, no problem, if this voltage drop <3.25V, the overtemperature signal will keep coming.

Richard Li
Senior
October 17, 2024

I missed one point, if Microchip voltage <3.3V, it can't keep gate drive work.

Sau_rusAuthor
Associate
October 17, 2024

Voh of microcontroller is mentioned as 3V that's why you are telling, this will not work?

Can u tell me any equivalent part of gate driver with same package?

Peter BENSCH
ST Technical Moderator
October 17, 2024

VNQ860SPTR-Evis not a gate driver, but a quad channel high-side driver.

What do you actually really need?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Visitor II
October 22, 2024

I think you may be able to get the gate driver from the above microcontroller.