Skip to main content
kelvin23
Associate
July 17, 2005
Question

question about the output voltage of L6208

  • July 17, 2005
  • 1 reply
  • 528 views
Posted on July 17, 2005 at 06:32

question about the output voltage of L6208

This topic has been closed for replies.

1 reply

kelvin23
kelvin23Author
Associate
May 17, 2011
Posted on May 17, 2011 at 10:18

The supply voltage for L6208 is 13V

CP input : 2k HZ

step motor :42BYG016(a bipolar stepper---12V/0.3A)

but the output voltage in pin outA1 is only 5V(step motor work normally without load )

why is so low ?

as I set the supply voltage on 24V

the output is about 11V

and the circut is the one in the L6208's application note

the output voltage what I expected in this circut is 10-12V when the supply voltage is 12-15V

another question is :how to increase the output voltage for the step motor and what parameter in L6208 decide the output voltage ?

[ This message was edited by: kelvin9527 on 17-07-2005 10:17 ]