Skip to main content
Zheng Liang
Associate III
July 17, 2017
Question

powerstep01 with high voltage design

  • July 17, 2017
  • 1 reply
  • 488 views
Posted on July 17, 2017 at 11:41

I'm using 

http://www.st.com/content/st_com/en/products/ecosystems/stm32-open-development-environment/stm32-nucleo-expansion-boards/stm32-ode-move-actuate-hw/x-nucleo-ihm03a1.html

 to evaluate the powerstep01 chip, and learn the design around the chip on PCB, but the MAX Voltage is confusing me to design with components. the evaluation board is printed with '50V MAX', but I checked the BOM, and found that the rating voltage of capacitors connected with VS are 100V, could this board run with 80V?(I have only one board shipped from USA, it will take long time on shipping for new one if I damaged this one). If not, what limit the MAX Voltage of this board?

Is there exist the possibility of spike on VS from motor with auto-adjusted current mode or voltage mode?

If I wanna drive with highest voltage of this chip, how much the rating voltage of capacitors should I used, 100V or 160V ? and how to chose the value of capacitor for the motor runing, something else should I be noticed in this design?

Thanks,

Zheng

This topic has been closed for replies.

1 reply

Zheng Liang
Associate III
July 19, 2017
Posted on July 19, 2017 at 08:14

Is there anyone run this

evaluation board 

above 80V? or some suggestions?