Skip to main content
ahagh.1
Associate
Nov 9, 2021 4:31 AM UTC
Solved

powerstep01_target_config generated by SPINFamily tool

when I use powerstep01_target_config generated by  SPINFamily tool on 401re the speed profile run 10 times faster that it runs on SPINFamily tool. I also change sys clock speed but no luck. please let me know if there is a solution to my problem.

and also is there any source code or example of this file Guifw-STM32F4xx-Nucleo.bin

thanks

This topic has been closed for replies.
ahagh.1
ahagh.1Best answer
Associate
Nov 15, 2021 1:28 AM UTC

HI @Enrico Poli​ 

I found out what is causing this problem, because I was using current mode I only update the current section of powerstep01_target_config

there for old parameter from section of Voltage mode parameters was used and it had different values from my motor.

generated file from SPINFamily tool need to replaced completely.

I also saw if I use BSP_MotorControl_Init(BSP_MOTOR_CONTROL_BOARD_ID_POWERSTEP01, &initDeviceParameters);

it will use Voltage mode parameters from powerstep01_target_config.

it is best to replace config with generated one

4 replies

Enrico Poli
ST Employee
Nov 12, 2021 3:40 PM UTC

Hello @ahagh.1​,

Welcome to the community.

Could you please share the powerstep01_target_config.h file generated by the SPINFamily tool and describe with more details the mismatch you found in the motor speed?

About the "Guifw-STM32F4xx-Nucleo.bin" firmware, it manages the interfacing between PC and POWERSTEP01 SPI communication.

Sorry, but the source code is not available.

Enrico

ahagh.1
ahagh.1Author
Associate
Nov 13, 2021 12:50 AM UTC

Hello @Enrico Poli​  and thank you for reply,

For example i want spin motor 360 at the speed i want, i use  SPINFamily tool in Current mode and set parameters at Speed profile section.

it spin the way i want .

/**************************** Speed Profile *********************************/
/// Register : ACC
/// Acceleration rate in step/s2, range 14.55 to 59590 steps/s^2 
 #define POWERSTEP01_CONF_PARAM_ACC_DEVICE_0 (8003.55)
 
/// Register : DEC
/// Deceleration rate in step/s2, range 14.55 to 59590 steps/s^2
 #define POWERSTEP01_CONF_PARAM_DEC_DEVICE_0 (8003.55)
 
///Register : MAX_SPEED
/// Maximum speed in step/s, range 15.25 to 15610 steps/s
 #define POWERSTEP01_CONF_PARAM_MAX_SPEED_DEVICE_0 (1297)
 
/// Register : MIN_SPEED 
/// Minimum speed in step/s, range 0 to 976.3 steps/s
 #define POWERSTEP01_CONF_PARAM_MIN_SPEED_DEVICE_0 (0)
 
/// Register : FS_SPD 
/// Full step speed in step/s, range 7.63 to 15625 steps/s
 #define POWERSTEP01_CONF_PARAM_FS_SPD_DEVICE_0 (15624.98)
 
/// Register : FS_SPD - field : BOOST_MODE 
/// Boost of the amplitude square wave, enum powerstep01_BoostMode_t
 #define POWERSTEP01_CONF_PARAM_BOOST_MODE_DEVICE_0 (POWERSTEP01_BOOST_MODE_OFF)

but when i use this parameters powerstep01_target_config or even change it with API commands motor stalls it is too fast,

for example if i change #define POWERSTEP01_CONF_PARAM_MAX_SPEED_DEVICE_0 (1297) to 200 and 8003.55 to 500

it is kind of going to be the speed that i want but it make motor jerky because it is not correct parameters.

i use en.x-cube-spn3_v1.6.0 example to spin the motor and i think the pulse this example is generating is too high and it run faster.

at least if we know what board setting is used in Guifw-STM32F4xx-Nucleo.bin we can use same parameters inside the code.

thanks

ahagh.1
ahagh.1AuthorBest answer
Associate
Nov 15, 2021 1:28 AM UTC

HI @Enrico Poli​ 

I found out what is causing this problem, because I was using current mode I only update the current section of powerstep01_target_config

there for old parameter from section of Voltage mode parameters was used and it had different values from my motor.

generated file from SPINFamily tool need to replaced completely.

I also saw if I use BSP_MotorControl_Init(BSP_MOTOR_CONTROL_BOARD_ID_POWERSTEP01, &initDeviceParameters);

it will use Voltage mode parameters from powerstep01_target_config.

it is best to replace config with generated one

Enrico Poli
ST Employee
Nov 15, 2021 1:59 PM UTC

Hi @ahagh.1​ ,

Glad to read you found the solution and thanks for sharing it with the community!

Kind Regards

Enrico