Skip to main content
Visitor II
October 6, 2025
Question

powerstep01 (stepper motor skipping steps after few hours of operation)

Which alarm to read if our motor skips steps while moving?

The motor works fine for a period of time like for 4hours and then randomly starts to skip step while moving in forward direction whereas in backward direction it moves fine. We are using 1/4 step mode. Below are the parameters we have inputted:-

POWERSTEP01_CONF_PARAM_KVAL_ACC_DEVICE_0 (48.5)

POWERSTEP01_CONF_PARAM_KVAL_DEC_DEVICE_0 (48.5)

POWERSTEP01_CONF_PARAM_KVAL_RUN_DEVICE_0 (45)

POWERSTEP01_CONF_PARAM_KVAL_HOLD_DEVICE_0 (16.02)

This topic has been closed for replies.