Skip to main content
michael gra
Visitor II
March 9, 2018
Question

powerstep01 spi baudrate setting problem

  • March 9, 2018
  • 0 replies
  • 463 views
Posted on March 09, 2018 at 14:05

Hello,

we tried to communicate to the powerstep01 trough spi and with a baudrate of 500kHz everythink works fine.

The problem occur if we set the baudrate above 500kHz. Then we lose the first bit of each byte.

For example:

   - send 0xFF to the powerstep01 ABS_POS and we receive as result 0x7F

   - send 0x1FF to the powerstep01 ABS_POS and we receive as result 0x17F

In the manual description is a max Value of 5MHz defined.

Somebody help me if i overlooked something or there have to be specific timing issues.

This topic has been closed for replies.