Skip to main content
GoA
Associate
Feb 24, 2022 1:40 PM UTC
Solved

POWERSTEP01. Is there a way to switch cleanly between MOVE and RUN?

3 Powersteps -> 3 steppingmotors for X, Y and Z axes, voltage mode.

Is there a way to switch cleanly between MOVE and RUN commands?

Currently, when I execute RUN command after MOVE movement, motors move too slowly. Although I change the speed (target - acceleration from 0 to 1200 RPM).

MOVE alone works fine, RUN curves without MOVE also clean.

Of course I wait for SMCMD_READY, and only then I send next command with SPI.

This topic has been closed for replies.
GoA
GoABest answer
Associate
Mar 1, 2022 7:09 AM UTC

This was interface error . Problem solved

2 replies

GoA
GoAAuthorBest answer
Associate
Mar 1, 2022 7:09 AM UTC

This was interface error . Problem solved

Peter BENSCH
ST Technical Moderator
Mar 1, 2022 7:46 AM UTC

Thank you for letting us know!

However, you are also welcome to post more details about the temporary misbehaviour so that other users can avoid it. Thank you!

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.