Skip to main content
CTapp.1
Senior III
May 8, 2024
Question

PowerSTEP01 - is the ResetDevice command conditional?

I have a PowerSTEP01 that is behaving unexpectedly when I send the ResetDevice command.

If I send it when my system starts then everything is ok when I check the STATUS register.

However, if I send ResetDevice after the motor has been moved (sequence ends with a SoftStop), then the status reports CMD_ERROR. Adding a status check shows that the error was definitely caused by the ResetDevice command - status before is 0xE012 and after is 0xE092.

This does not happen if I issue a HardHiZ before the ResetDevice.

This topic has been closed for replies.