Peter BENSCHBest answer
ST Technical Moderator
March 5, 2026
Welcome
Your understanding of the T0/T1/T2 encoding with CLS1 = 36.5Ω and CLS2 = 51.1Ω resistors is correct: for a Type 2 (PoE+) PSE the PM8805 should report 'T2:T1:T0 = 1:1:0', as shown in line 2 of table 10 of the data sheet.
The fact that PGD is asserted but all T0...T2 lines stay high (LEDs off on STEVAL-POE001V1 and your own board) suggests that the PM8805 does not detect the PSE as an IEEE‑802.3af/at/… compliant source, but rather as a legacy / passive injector or in a non‑standard mode.
To investigate further, could you please share:
- the exact test setup (cabling, injector mode/settings, power level),
- scope screenshots of VPORT and the CLS1/CLS2 pins during startup,
- confirmation that the injectors are set to 802.3af/at mode (not “passive PoE” or vendor‑specific mode)
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.