Skip to main content
Associate
May 14, 2024
Question

pincount

could you help me to get pincount for part number   ''   STPSC6H065DLF  ''  

 

Pin Count for this PN "" as supplier site mentioned it as "4" while it's found in datasheet as "5"?

This topic has been closed for replies.

4 replies

Peter BENSCH
ST Technical Moderator
May 15, 2024

I assume you are referring to MLPD 8X8 4L with the statement about 4 pins, which can be found on the product website and the tab Sample & Buy?

Well, you have to be careful in which context you talk about pins and connections, which can unfortunately lead to confusion. In this case, the package indeed has 4 pins, which are led to the package edge with bond wires. However, it has 5 electrical connections because the cooling slug is also used to connect the cathode.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
May 15, 2024

thanks for your reply

But i need ask , Is it  applicable to connect exposed pad or cooling slug  to Main pin as cathode ?

Andrew Neil
Super User
May 15, 2024

@mohamed_badran wrote:

Is it  applicable to connect exposed pad or cooling slug  to Main pin as cathode ?


According to the datasheet, the exposed pad is the only connection to the cathode:

AndrewNeil_1-1715761718965.png

 

So, if you don't connect to that, you won't have any connection to the cathode at all !

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.