Skip to main content
Explorer
May 23, 2025
Solved

Pin Layout Difference and Equivalent IPM for STGIB8CH60TS-E

We are currently evaluating two ST IPM modules for our motor drive applications — STGIB8CH60TS-E and STGIB15CH60TS-L. Upon reviewing both datasheets, we noticed that although the two devices share the same functional pin descriptions where (STGIB8CH60TS-E have max current of 12A @ 25°C) and (STGIB15CH60TS-L  have a max current of 20A @ 25°C) but package types are different, the physical layout of certain pins, specifically Pin 19 (NV), differs between the two modules.

We would appreciate your clarification on the following points:

  1. What is the technical reason for the difference in Pin 19 layout between the STGIB8CH60TS-E (Type E package) and STGIB15CH60TS-L (Type L package)?

  2. Are there layout-compatible alternatives to STGIB8CH60TS-E (i.e., IPMs with similar electrical characteristics and identical physical pin positions) that could support higher current or allow for flexible sourcing?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 23, 2025

Welcome @VishnuNatarajan, to the community!

  1. The extended pin 19 was probably introduced at the time at customer's request.

  2. The STGIB8CH60TS-E is the only remaining variant with this layout in the portfolio of STMicroelectronics.

Does it answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 23, 2025

Welcome @VishnuNatarajan, to the community!

  1. The extended pin 19 was probably introduced at the time at customer's request.

  2. The STGIB8CH60TS-E is the only remaining variant with this layout in the portfolio of STMicroelectronics.

Does it answer your questions?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.