Skip to main content
ACell.1
Visitor II
August 4, 2021
Question

Part STM6904 Doc ID 14289 Rev 3 Pull-up on /rst output open-drain in Table 2. Signal names and functions on 8 RST Output Active-low open drain reset output (10 kΩ internal pull-up) I think the note (10 kΩ internal pull-up) was meant for pin 1

  • August 4, 2021
  • 0 replies
  • 577 views

From the rest of datasheet and also from the test we have performed preparing a test circuit it looks like there is no pull-up on the output (as it should be for an open drain), if so please update the datasheet. Please confirm if we are right or otherwise please give further detail.

Some samples of STM6904SFEDS6F will be appreciated for the time lost in doing the tests. Thanks

    This topic has been closed for replies.