Skip to main content
victagayun
Senior III
Mar 12, 2021 4:24 PM UTC
Solved

P-Nucleo-IHM001 Motor Not rotating

I have ordered P-Nucleo-IHM001 via Digikey.

When trying the default FW, both FOC and 6-steps, the motor is not rotating.

I connected the motor to a drill and rotate it, all three wires will produce around 1V peak to peak.

Here is the video when testing.

https://www.youtube.com/watch?v=3GXGae1relg

Any idea which one is faulty? Motor, driver board, etc?

This topic has been closed for replies.
victagayun
victagayunBest answer
Senior III
Mar 23, 2021 11:27 PM UTC

Hi,

Sorry for the late update.

The motor stuck because of tight mounting on the PCB and hole misalignments.

The base of the motor slightly warped due to tension and it cannot rotate due to friction.

Thanks!

4 replies

victagayun
Senior III
Mar 13, 2021 12:07 AM UTC

I also tried Motor Profiler App, it would take a long to test and will fail.

I also measured by current probe with amplifier, there is an AC current with same amplitude and freq for each wires.

Cristiana SCARAMEL
ST Employee
Mar 23, 2021 5:18 PM UTC

Hello @victagayun​,

in your video the led D11 on X-NUCLEO-IHM07M1 is blinking twice so you are in FOC control mode (JP1 and JP2 closed, J5&J6 on 3Sh side).

I cannot check all the NUCLEO-F302R8 settings:

  • JP1 open: ok
  • JP5 (PWR) on E5V side: it seems to be open (please check)
  • JP6 (IDD) closed: it is no visible, please check.

Can you confirm that you have made all the settings before applying the 12 V power supply?

Have you tried regulating the motor speed via the potentiometer (R42)?

For a better support, please check the above settings and share feedback.

"If you feel a post has answered your question, please click ""Accept as Solution"""
victagayun
victagayunAuthorBest answer
Senior III
Mar 23, 2021 11:27 PM UTC

Hi,

Sorry for the late update.

The motor stuck because of tight mounting on the PCB and hole misalignments.

The base of the motor slightly warped due to tension and it cannot rotate due to friction.

Thanks!

Cristiana SCARAMEL
ST Employee
Mar 24, 2021 8:16 AM UTC

Hi @victagayun​,

thank you for sharing the resolution to your problem.

"If you feel a post has answered your question, please click ""Accept as Solution"""