Skip to main content
elektronika
Associate
August 30, 2016
Question

No stabilization of output voltage | SPV1040

  • August 30, 2016
  • 1 reply
  • 873 views
Posted on August 30, 2016 at 19:21

Hi.

I designed the power converter which is supply from the photovoltaic cell ( Umax = 5.5 V / 1 W) on a SPV1040. The problem is that the system did not stabilize the output voltage.The output voltage is proportional to the input voltage.

I attach the schematic:

0690X00000602gXQAQ.jpg

Someone sees what mistake I make?
This topic has been closed for replies.

1 reply

elektronika
Associate
August 30, 2016
Posted on August 30, 2016 at 19:43

I forgot to add that I no soldering diodes D1 and

D2. :)