Skip to main content
sales
Visitor II
October 26, 2014
Question

Need recommendation for Full Bridge Driver

  • October 26, 2014
  • 0 replies
  • 439 views
Posted on October 26, 2014 at 05:55

I need a Full Bridge driver IC capable of at least 2.5 Amps at 125 kHz.

The L6225 connected in parallel looks good but the highest frequency is only rated to 100 kHz

Is there a higher frequency version of this or can it be driven ok at higher than rated switching frequency?. 

Thanks

#h-bridge #full-bridge-driver
This topic has been closed for replies.