Skip to main content
Visitor II
October 7, 2024
Question

Need DPAK MOSFET with high avalanche rating

We've been using the On Semi FDD8453LZ MOSFET (40V, 6.7 ohm, DPAK) in our motor control designs for many years, but this part is now EOL.  We're looking for a suitable DPAK replacement.  One critical parameter is the single pulse avalanche energy, which must be equal or better than the FDD8453LZ's 253 mJ.  Unfortunately this is not a parameter that normally is listed in parametric selection tables.  Does ST have a 40V DPAK MOSFET that meets this requirement?

Thanks,

Mark 

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
October 7, 2024

Welcome @WiscEng, to the community!

what about e.g. the STD120N4F6 with 394mJ in DPAK?

Regards
/Pete

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.