Skip to main content
Nandish Jasani
Associate
Dec 5, 2019 2:56 PM UTC
Solved

Need ACIM Evaluation kit

Hi,

I am looking AC Induction motor evaluation kit. I have worked experience with STM32F4 and STM32F7 series microcontroller. So i need to make AC Driver for AC Induction Motor with all Four Quadrant operation. So please suggest me the AC Induction motor evaluation kit from ST which can interface with any STM32F4 or STM32F7.

Also suggest me the compatible ACIM motor with that evaluation kit.

Thanks in Advance.

Regards,

Nandish Jasani.

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:53 PM UTC

Dear @Community member​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

1 reply

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:53 PM UTC

Dear @Community member​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards