Peter BENSCHBest answer
ST Technical Moderator
Jan 14, 2021 9:25 AM UTC
Hi, @AZata.2393 ,
thanks for this interesting question.
As you said, the datasheet actually shows the marking for both packages SO-8 and PowerSSO-16, as well as the order codes on pg 39. The TR suffix is well known throughout the industry as "Tape and Reel". Because only two packages are available, which can also be distinguished with a unique letter (J/S) within the ordering code and simply by looking at them, the 7 characters mentioned are fully sufficient for identification.
Hope this helps in communicating to the customer?
Regards
/Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.