Motor spins and triggers a fault with STSPIN32F0A and the SPIN3202 6-step library
- January 2, 2019
- 1 reply
- 835 views
A few Qs about the 6-step library. I have a 350W, 36V motor that I'm trying to control using the STSPIN32F0A. I've got the 6-step library working ... sort of. The motor rotates for a few moments and then a fault state is triggered (USER2 LED). In the short time the motor rotates, the RPM does not match what is defined in the motor spec sheet header file. Also, I do not see any zero crossing and commutation event monitoring on PA5 and PA15 and I have enabled those in the motor header file.
As stated in the guide, I've lowered the ACC value way down to 60. I have enabled the voltage mode in the defines and I'm using hall sensors for the commutation process. I've attached the motor spec .h file here.
First Q: Not sure where to start debugging. As per the guide (pg. 32), I know that the RPM of my motor needs to be ~150. The motor has 15 pole pairs and with this value, I calculated the step-time to be 4.4ms. Based on this I calculated the LF_TIMxduration. Using the LF prescaler of 24 and a system clock of 48MHz, I get LF_TIMxduration to be 8800 counts. I'm guessing this is the LF_TIMx_ARR value in the motor spec .h file. Is this the right way to calculate this?
Second Q: How do I start tweaking the PI values?
Here are the defines:
USE_HAL_DRIVER,STM32F031x6,NO_UART_COMM,NO_PID,HALL_SENSORS,NO_ALL_WINDINGS_ENERGIZATION,NO_FIXED_HALL_DELAY,NO_PWM_ON_BEMF_SENSING,NO_MC_FAN_4PP_24V,NO_MC_RS_57BL54,NO_MC_2036_U_024_B_K312,NO_MC_BR2804_1700_KV_1,MC_360W_36V_BLDC,COMPLEMENTARY_DRIVE,VOLTAGE_MODE,POTENTIOMETER,NO_CURRENT_SENSE_ADC,NO_VBUS_SENSE_ADC,NO_TEMP_SENSE_ADC,NO_BEMF_RECORDING,NO_SPEED_SENDING,NO_SPEED_RAMP