Skip to main content
peterdonchev
Senior
March 21, 2018
Question

Motor Control Library maximum modulation index

  • March 21, 2018
  • 0 replies
  • 547 views
Posted on March 21, 2018 at 10:37

Hi,

I have question about maximum modulation index in motor control library. When it is 100% is there any danger at very low RPM high side driver's bootstrap capacitors to be completely discharged? Is there any mechanism which guarantee that low side of the half bridge will be switched on in predefined interval of time?

#modulation-index #motor-control-library
This topic has been closed for replies.