Skip to main content
HDono.1
Visitor II
Jun 22, 2022 6:37 PM UTC
Question

Maximum Output capacitance for STBB3JR. What is the recommended upper limit cor ceramic capacitors?

..

    This topic has been closed for replies.

    1 reply

    Peter BENSCH
    ST Technical Moderator
    Jun 23, 2022 6:47 AM UTC

    Welcome, @HDono.1​, to the community!

    There is only a recommended minimum of 10µF for both the input and output capacitors, which should also be ceramic because of the lower ESR.

    What capacitance would you want to use?

    Regards

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.