Skip to main content
Associate
November 8, 2024
Question

Low Input Voltage to AEK-POW-BMS63EN

Hello,

The AEK-POWBMS63EN is a Battery Management System. I am not sure if I can connect to a voltage lower than 48V, if yes, would it work optimally? What issues I might come into?

Please kindly advise

shafkat_0-1731087709589.png

 

This topic has been closed for replies.

3 replies

Peter BENSCH
ST Technical Moderator
November 8, 2024

The description is a little misleading, the 48V refers to a single block consisting of up to 14 Li-Ion cells, which have a maximum total of 48V. You can of course also charge one single cell.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
shafkatAuthor
Associate
November 8, 2024

Thanks Peter for responding!

So what does the 800V mean?

Peter BENSCH
ST Technical Moderator
November 10, 2024

800V means many blocks (nodes) in series, each one with a dedicated L9963 able to handle 4…14 Li-Ion cells.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.