Skip to main content
Associate
February 12, 2025
Solved

LED7708 Random LED switch off issue with driver

Our requirement was to create a LED driver circuit to power 12 strings of 7 LEDs from a 12V DC supply with a nominal current of 20mA per string.
Using the STEVAL-ILL035V1 Development board data for PCB layout guidance and the LED7708 design tool spreadsheet for component selection we successfully built a prototype driver PCB and produced firmware to setup the on-board registers and control the LEDs for our application.

Initial results were good and all appeared to be working as expected until we noticed that after a random period (5 to 10 minutes) the LEDs would go off completely and wouldn't recover normal operation untill the device was disabled (DEVCFG0.DEN = 0) and then re-enabled.

When the LEDs go off the boost converter goes into a skipping mode of operation but no errors are indicated either from the XFLT pin or the status registers.

After disabling/enabling the device, the LEDs would come back on normally but would then go off again some time later. Interestingly this would be a much shorter period than the initial illuminated period. I'm unsure if this indicates a heat issue but temperature measurements (taken at 25DegC ambient) of the LED7708 device and PCB don't show anything outside expected running temperatures.

If the LED brightness is lowered from 100% to below 75% or the number of enabled strings is reduced this appears to have an effect on how long they will stay illuminated. Sometimes they will stay on indefinitely at 50% dimming.

If anyone has had issues like this in the past, maybe you could tell us about your experiences or possible solutions you can suggest.

Many Thanks,
Shapeshifter

This topic has been closed for replies.
ShapeshifterBest answer
Associate
February 18, 2025

Hi Peter,

Thanks for looking into the shutting down issue we were experiencing with the LED 7708 device.

I believe we have now identified the cause of the problem which was partially temperature related but not quite what we originally suspected.
I think its useful to let you know how the problem originated so others trying to use the device may proceed more cautiously and not run into similar issues.
As I noted in my initial post, we used the LED7708 design tool spreadsheet for component selection which offers up suggested values for many parameters to get you started and lets you optimise them for your application. Unfortunately the spreadsheet allows you to change parameters without giving warnings that you may be moving outside of working range.
We fell foul of this while setting up the internal dimming oscillator's external setting resistor value. The resistor value range is buried in the datasheet and at first it wasn't entirely clear whether the values sited were examples or the working range. This meant that the calculated value offered by the spreadsheet, that we used, was too large and outside the working range.
We now believe that the dimming oscillator was starting up when the device was at room temperature but then failed when the temperature rose to the operating temp of around 40degC and caused the LED outputs to shut down.

Hopefully this solution will prove helpful to any interested parties.

Thanks again,
Shapeshifter.

7 replies

Peter BENSCH
ST Technical Moderator
February 13, 2025

Welcome @Shapeshifter, to the community!

I am quite sure that you have a heat problem. As you describe, the tests (including long-term tests?) with the STEVAL-ILL035V1 were successful. What are the differences between the EVAL and your board?

Which components do you use for the boost stage (L, T, D, C output)?

What does your layout look like, especially under the LED7708?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
February 13, 2025

Hi Peter, many thanks for picking up our design problem

To give you a bit more general info on our design, I've attached the schematics of the Drive cct, together with the PCB layout.

The main components are:
Input Caps: 56uF Elec together with 2x 4.7uF 50V ceramics
Inductor: 22uH Isat 1.6A (Bourns SRR6038)
FET: 30V 8A (Diodes DMG4466SSS)
Diode: Schottky 60V 1A Vf 0.5V (ST STPS1L60)
Output Caps: 2x 10uF 50V ceramics

Driver SchematicDriver Schematic

LayoutLayout

Copper bottomCopper bottom

Copper topCopper top

 

Main design parameters, as used in the spreadsheet:
- Input voltage 12V +/- 10%
- 12 channels, each comprising a string of 7 LEDs, Vf 2V - 2.6V, Iled 20mA
- Expected output voltage; Vdrive 14V - 19V
- typical Dccm ~0.3
- Output power; Pout < 4.5W

The problem symptoms, of the LEDs turning off after a period, feel temperature related. However none of the calculations and measurements suggest there is a power dissipation problem.
The spreadsheet suggests a Pdchip of 480mW, Tj 42degC. Measurement with a thermal camera gives ~44degC.

 

Peter BENSCH
ST Technical Moderator
February 13, 2025

If I take a closer look at your layout, I can see the 13 thermal vias on the blue rear side, which transport the heat from the LED7708 there. However, the GND area there is separated by two tracks, which reduces the heat transport in the area to perhaps 25% of the possible value. The STEVAL-ILL035V1 also has a few tracks around it, but at a greater distance, so that the heat flow is less impeded. Additionally the EVAL uses 16 thermal vias instead of 13. However, as your thermal imaging camera only measures 44°C, this may not be a problem.

BTW: what is the status of XFLT and the DEVCFG0 register in the event of the shutdown?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.