Skip to main content
Erik de Wit
Associate
January 30, 2020
Question

LED6000 use DIM as enable

  • January 30, 2020
  • 0 replies
  • 664 views

Hi all,

The LED6000 has a seperate EN and DIM line. I would like to use the dimming feature and also be able to disable the device. It seems I could use DIM only, and tie EN to VCC. Then, if I hold DIM low, the device should be disabled. As I use multiple drivers in my design, I only need 1 line per driver from the microcontroller.

Does anyone know if this is correct?

This topic has been closed for replies.