Skip to main content
Visitor
Nov 23, 2026 12:17 PM UTC
Question

L9965A: cell balancing with external MOSFETs driven from the Sx pins?

Hello,

The L9963E datasheet (DS13636 §6.6.2, Fig. 38) describes balancing with external NMOS/PMOS FETs driven from the Sx pins. Is the same approach supported on the L9965A / L99BM218? I could not find it in DS15021 or AN6387.

The L9965A has one S pin per cell tap, with the internal FET between Sx and Sx-1. The L9963E circuit would therefore need to be adapted. Every second S pin would act as a "gate" pin, connected to the tap through a drive resistor and driving the PMOS of the cell below and the NMOS of the cell above. The other S pins would be "common" pins, connected to the tap through a low resistance. Odd/even swap would keep the two channels that share a gate pin from being on at the same time.

  1. Is external-MOSFET balancing supported or validated on the L9965A? Is there an application note or reference schematic?
  2. During the open-load diagnostic, IBAL_DIAG flows through the drive resistor. Is there a recommended maximum value, and does the balance-open diagnostic still work?
  3. Are IBAL_DIAG currents still injected on S pins of channels masked with VCELLx_EN = 0 or VCELLx_BB = 1?

Thank you.