Skip to main content
GLasw.1
Associate
May 18, 2020
Question

L9963 BMS IC Programming Document and other informations

  • May 18, 2020
  • 0 replies
  • 746 views

Hi ST,

I am interested In using the L9963 IC for UPS battery management system.

Since it is a UPS, i am not intending to use the default SPC574S64E3 but another STM32 MCU.

The following are my questions:

  1. Is there any Programming Manual for the L9963 IC as i have searched and found none currently?
  2. Since it has an ISO and SPI interface, can i use another STM32 MCU for communication with the L9963 using the SPI interface or use the L9963T transceiver?
  3. If i where to test the IC using the UM2698: EVAL-L9963-MCU Evaluation Board, where can i get the STSW-L9963 PC Graphical User Interface Software?
  4. The evaluation board in 3 above, has the L9963T transceiver IC, but i can not find any information on the IC through the ST Website, where can i get information of this IC or where can i purchase it?

Thank you in advance.

This topic has been closed for replies.