Skip to main content
jdiogo10
Visitor II
August 8, 2013
Question

L9942 - Motor lose some microsteps

  • August 8, 2013
  • 3 replies
  • 1096 views
Posted on August 08, 2013 at 20:17

I want to control a stepper motor (

http://pt.farnell.com/astrosyn/163/stepper-motor-1-8deg-5v/dp/9598650

) with L9942 from ST.

But i have some problem because the motor dont rotate uniformly (lose some step):

0690X000006057MQAQ.png 

My current profiles are (for DC = 111 - 1300mA):

0690X00000605RhQAI.png

Can you help me? Why lose some step?!

#l9942-stmdiscovery-stm32f4
This topic has been closed for replies.

3 replies

Brugus
ST Employee
February 2, 2014
Posted on February 02, 2014 at 19:41

The STEP signal is an input signal and it should be generated by a microcontroller or by an external circuitry.

Checking the scope-snapshot, the duty cycle of the STEP signal is not constant. this behaviour can be the source of the problem you claimed.

thomas239955
Visitor II
July 9, 2014
Posted on July 09, 2014 at 21:22

Good morning,

I would like to know how you manage to use the SPI protocol with the L9942 driver. I doesn't manage to use it so far...

Thank you in advance,

Thomas.

Brugus
ST Employee
July 14, 2014
Posted on July 14, 2014 at 18:19

dear Thomas,

The info you need are reported in the datasheet

Please check chapter 5 and 6. Figure 10 and figure 11 are showing the timing diagrams.

Best regards,

Marco.