Skip to main content
Sourabh Joshi
Associate
April 24, 2017
Question

L9823 as Input?

  • April 24, 2017
  • 2 replies
  • 738 views
Posted on April 24, 2017 at 13:15

I am using L9823 in my design to drive the outputs. I also want it to behave as input so that I can connect IO module. How can I use it as input?

Thanks in advance

This topic has been closed for replies.

2 replies

Luigi DI-TURI
ST Employee
May 15, 2017
Posted on May 15, 2017 at 14:13

On top of what is reported in the DataSheet, what is not clear? Please, could you better specify what is unclear?

Thanks for your feedback

Best Regards

Luigi

Sourabh Joshi
Associate
May 16, 2017
Posted on May 16, 2017 at 05:22

As L9823 is an output driver IC, I wanted to use it as input also. I need to connect IO devices in my design on same line. i.e. the user can change the module as per his requirement from Input to output or vice versa. As L9823 is an output driver IC, I don't want to use separate hardware for Input detection in case input module is connected. So I am thinking of using fault detection feature as input. 

Is it a good design to use fault detection feature as input?

Thanks for the feedback.

Regards,

Sourabh