L6981(C50DR) dies on hard switching of input power
- 6 replies
- 546 views
Hello everybody,
I'm using an L6981C50DR for supplying a small board with 5V. The schematics is attached and should be perfectly conform to what is described in the specification from https://www.st.com/resource/en/datasheet/l6981.pdf as "Figure 4. Basic application (fixed VOUT versions)" on page 3. I'm supplying 24V to it. Everything works well when I turn on and off the power via the switching power supply that provides these 24V. But when I reboot my board the "easy way" by pulling out and reconnecting the +24V wire, the L6981 dies immediately. After this, pin 4/Vout is permanently at GND letting me assume something has melted within the IC.
When measuring the switching power supply with an oscilloscope, it provides a small peak in such a scenario but this peak does not go beyond of 28V - which is far below the 40V the L6981 should be able to deal with.
So...any ideas what the reason for this problem is and how to solve it?
Thanks!