Skip to main content
Visitor II
May 15, 2025
Question

L6599A Shutdown

Hello.

I'm using L6599AD without PFC.

Previously, the DIS pin was connected to the delay pin and used as a shutdown.
However, frequent peak current caused shutdowns.
So I connected DIS pin to GROUND and made it work in HICCUP mode.

However, the problem is that there are still occasional shutdowns.
When I was using it in HICCUP mode, shutdown occurred and when I checked, PFC_STOP pin was in LOW state. (ISEN pin is OPEN state, pull_down.)

With the ISEN pin OPEN, how can I get to the PFC_STOP pin in the LOW state?

What are some situations where PFC_STOP can be shut down in the LOW state instead of overcurrent?

It's a frustrating situation to have such a problem.
Please help me.

This topic has been closed for replies.