Skip to main content
dziulijus
Visitor II
June 1, 2016
Question

L6482H settings.. What I'm doing wrong?

  • June 1, 2016
  • 0 replies
  • 506 views
Posted on June 01, 2016 at 09:04

Hello guys,

I have been working on stepper controller board using L6482 chip, but with no luck making it to work..

Problem: I'm getting over-current fault when I try to drive the motor (motor doesn't make any movement).

Controller settings:

TON_MIN = 4us,

TOFF_MIN = 21us,

TOFF_FAST = 10us,

FAST_STEP = 16us,

TSW = 48us,

Predictive current control is ON,

Gate current = 16mA,

VCC value = 15V,

UVLO tresholds = 7V,

Turn OFF boost time = Disabled,

Controlled current time = 1500ns,

Blanking time = 500 ns,

Dead time = 250 ns,

All currents set to 195.31mV,

Over-current treshold = 750mV.

Power supply = 36V, 11A (SMPS)

Mosfets I'm using:  IPP180N10N3G, Qg= 19nC (25nC max)

Stepper: Nema 23, 0.9 Ohms, 3.8 mH.

I need to deliver max 4.5 Amp to the motors. Speed should be around 400steps/s at 1/16 microstepping.  I have tried to set very low current setings for the motor but stil nothing is happening.. PCB is made with using EVAL 6482 as a reference, only MOSFETs are different. 

Looking forward for your answer!

Thank you!

Julius K.

This topic has been closed for replies.