Skip to main content
cliang
Associate II
April 16, 2015
Question

L6480H driver stall detection and overcurrent detection

  • April 16, 2015
  • 1 reply
  • 536 views
Posted on April 16, 2015 at 16:16

In application note AN4355, overcurrent detection page 18 and stall detection page 21, application note writes two equations

Equation 1: I

OCDth

= V

OCDth

� R

ds(ON)

Equation 2: I

STALLth

= VSTALLth � Rds(ON)

Why current is equal to voltage times resistance?

should be use divide sign I

OCDth

 = V

OCDth

 � R

ds(ON)

How should I calculate overcurrent I

OCDth

 ?

for an instance, by default, I

OCDth

 is 281.25mV, and external MOSFET R

ds(ON)

 is 33m?, what is I

OCDth equal to ?

Thank you in advance

#ocd #l6480h #stall-detection-l6470
This topic has been closed for replies.

1 reply

Enrico Poli
ST Employee
April 27, 2015
Posted on April 27, 2015 at 09:49

You are right, the formulas of the AN are wrong.

The actual relation betwee programmed threshold and current is I

OCDth

= V

OCDth

÷ R

ds(ON)

The typo will be fixed in the next release of the AN. Thanks a lot for your feedback!

Regadrs

Enrico