Skip to main content
Phlip Cornelissen
Associate II
January 15, 2018
Question

L6480 absolute position counter value issue

  • January 15, 2018
  • 1 reply
  • 585 views
Posted on January 15, 2018 at 10:45

Hi

The L6480 absolute position counter seems to count in multiples of 256 micro steps? When executing the move command with a 1000 micro steps or using the GoToDir command with a 1000 micro step value both generate a motion that ended in having a value of 256000 int the absolute position counter. When I reverse the direction the value is -256000 as expected, or should I say not expected! This count in multiples of 256 is a constant count and is not affected by the choice of micro stepping mode. may it be 1/8, 1/16 or 1/32 makes no difference!

Why is this? Is there a different setting or configuration for this? Any ideas on how fix this? I want to read the true number of micro steps and not in multiples of some value.

Best regards

This topic has been closed for replies.

1 reply

Kurtnelle
Associate II
March 6, 2019

Something is wrong in your code.