Skip to main content
sburr
Associate II
October 2, 2014
Question

L6470H discovery Issues on two systems

  • October 2, 2014
  • 2 replies
  • 673 views
Posted on October 02, 2014 at 22:29

I am attempting to run the L6470H discovery kit with the dspin software from a machine with windows xp on it. I was previously able to run it from another machine with xp, I installed the same files but cannot connect to the board. I get a windows error with the following parameters:

EventType : clr20r3     P1 : gui.exe     P2 : 1.2.5071.18356     P3 : 528b2b58

P4 : mscorlib     P5 : 2.0.0.0     P6 : 4a7ce2b8     P7 : 1295     P8 : 14    

P9 : system.missingmethodexception    

On the other system I get an error with spi_dll when I connect, any ideas?

I have tried to download the latest software with no luck.

#l6470h #discovery-eval6470-disc
This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
October 3, 2014
Posted on October 03, 2014 at 16:03

Hi,

The SPINFamily software is based on the Microsoft .NET framework.

Please, check the installation of this component.

Regards

Enrico

sburr
sburrAuthor
Associate II
October 3, 2014
Posted on October 03, 2014 at 18:21

I installed 4.0 and I get the same error, this time it is delayed by a few minutes. do I need to install a different version of .net?