Skip to main content
rvanvreden
Associate II
Feb 26, 2018 2:16 PM UTC
Question

L6470 Cracked

Posted on February 26, 2018 at 15:16

L6472 stepper driver.

hello, we are using 4x L6472 driver chip on a single board for some time now. We used the internal 16MHz clock, but it appeared that the clock frequencies differ a lot from each other. According the specs it can be plus or minus 3%. With four motors running simultaneously, it looks a bit funny to see them running different speeds/s. So what we did is using an external clock source. This clock is generated by the attiny, so is only available after the tiny is up and running. This worked for a coupe of days.

now my question; this morning we blew up ( housing cracked open) 3 of the 4 L6470 while programming the Attiny. And we want to know why that happened? Also the boot diodes of three L6472 fried. 

Is this because the L6472 needs a clock before it can handle the init strings via SPI? I cannot find anything in the spect about the external clock and/or/if it must be present before the L6472 receives serial data?

Or, is there an other reason why three drivers fry? where to look at?

regards,

rob

This topic has been closed for replies.