Skip to main content
mahlers9
Associate
Aug 18, 2011 7:35 PM UTC
Question

L6470: connect Vreg and Vdd for 5V supply?

Posted on August 18, 2011 at 21:35

L6470: connect Vreg and Vdd for 5V supply?

#l6470 #l6470
This topic has been closed for replies.

4 replies

mahlers9
mahlers9Author
Associate
Aug 18, 2011 7:42 PM UTC
Posted on August 18, 2011 at 21:42

bille.stello
Associate
Aug 29, 2011 7:34 AM UTC
Posted on August 29, 2011 at 09:34

For 5V supply voltage:

VREG connected to 3.3V or  internally supplied (in this case plase a capacitor on Vreg pin)

VDD connected to 5V

joe239955_stm1
Associate
Jan 5, 2012 3:42 PM UTC
Posted on January 05, 2012 at 16:42

If using 5V only for Vdd

What value cap(s) are recommended for a open (using Internal 3.3V reg) Vreg pin

Thanks

Joe

Enrico Poli
ST Employee
Jan 10, 2012 9:43 AM UTC
Posted on January 10, 2012 at 10:43

Dear Joe,

The VREG pin needs at least a 22uF capacitor to be stable. The recommended value is 47uF.

If you want to use a electrolytic cap, I also suggest you to add a small ceramic cap (100nF) to filter the current spikes coming from the logic.

The VDD need a 10uF capacitor.

Kind Regards

Enrico